Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Friction-optimised bearings for propellers with folding mechanism in electric motor glider

Robust and vibration-reducing

An almost maintenance-free plain bearing with low coefficients of friction combined with aluminium F52 is designed to adjust the blades on a highly efficient propeller with a folding mechanism. The smooth-running and vibration dampening properties of iglidur® J were able to impress here. Furthermore, a search was made for a robust, cost-effective and maintenance-free solution for the rotary movement of the steering wheel. drylin® R solid polymer bearings provide the ideal solution here, as besides meeting the required properties they are also resistant to temperature.

Profile

  • What was needed: iglidur plain bearing, drylin shaft guides
  • Requirements: The bearings in the glider should be as maintenance-free, robust and cost-effective as possible, and at the same time have the lowest possible friction values.
  • Industry: Aerospace, aviation industry
  • Success for the customer: iglidur J and drylin R bearings offer the customer an ideal solution: They are vibration-dampening and lubrication-free, which also eliminates maintenance.
Electric motor glider

Problem

For this advanced electric motor glider for 2 persons, bearing products for various places were sought for the prototype. First of all, the pitch control of the planned high-efficiency propeller with folding mechanism required a plain bearing that had to be virtually maintenance-free. The planning envisaged the use of the bearing in combination with aluminium F52. The bearing should also have only low coefficients of friction. The second place for which a bearing was needed was the steering of the aircraft around the vertical axis. It is controlled via a rotary handle on the hand control. For this purpose, a robust, cost-effective and maintenance-free solution for the rotary movement was sought.

Solution

The pictures document the design principle and the implementation of the glider. For the pitch control, the designers opted for the vibration-dampening plain bearings made of the iglidur J material. They were also chosen because they are lubrication-free and therefore maintenance-free in use. For the control of the aircraft, one uses drylin R solid plastic bearings, a solution that is as simple as it is ideal for the application. The top bearing is coupled with an internal double potentiometer that supplies the required electrical signals. By covering the three bearings with an elastomer, a matching handle is created. The temperature resistance of the plastic bearings is important here. In addition, the bearings allow for fault tolerances when pressed with the elastomer.

Plain bearings
Plain bearings
Plain bearings

Wolfgang Liehmann, Silent Flight e.V., Weingarten



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH