Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Weatherproof plain bearings in reliable lowering mechanism for radiator mascot

Wear-resistant in cold and hot environments: iglidur clip bearings with lowering mechanism

On luxury cars such as the Rolls Royce Phantom, the radiator mascot can be retracted into the bonnet to protect against theft. With the mechanism used so far, the components (reworked flange bearings) did not lie evenly over the surface. They also had to be pressed in so that they do not get lost. With the use of iglidur clip bearings from igus, the mechanism could be improved. Their advantages are the consistent flange thickness and the high wear resistance in various environmental conditions such as cold, heat or fine Sahara sand.

Profile

  • What was needed: Clip bearing from the iglidur plain bearing product range
  • Requirements: The search was on for a favourable sliding surface with a constant flange thickness, which is very wear-resistant even in cold and warm environments and under the strong influence of fine Sahara sand.
  • Industry: Automotive industry
  • Success for the customer: The iglidur bearings enable the flat movement between the two metallic components and are perfect for outdoor use with their specifications such as low moisture absorption and resistance to temperature and corrosion.
Countersink

Problem

On luxury cars such as the Rolls Royce Phantom, the radiator mascot can be retracted into the bonnet to protect against theft. In the course of a re-modelling project, sliding surfaces were sought that were movable in relation to each other between two metallic components. In an early prototype, this was fulfilled by reworked flange bearings. It had to be pressed in so that it would not get lost. However, this had the disadvantage that the flange bulged out differently after pressing in and thus the components did not have a uniform surface contact.
What was needed for the implementation of volume production was a cost-effective sliding surface with an even flange thickness, which could be installed by hand, which was loss-proof, which could be used for two different material thicknesses (1-3 mm) and which was also very wear-resistant in cold and warm environments, even under the strong influence of fine Sahara sand.

Solution

The car manufacturer finally found the solution to the problem in our product range. To be more precise, the idea of using iglidur clip bearings came up, which significantly improved the mechanism. It was very important that the flange thickness of the bearings remained the same and that the desired flat movement between the two metallic components was possible. But the other specifications of the iglidur material could also solve some problems in this application. For instance, it is characterised by its low moisture absorption as well as exceptional resistance to temperature, chemicals and corrosion. The features of the bearing products thus make the components the ideal solution for use in severe weather conditions such as cold, heat, humidity or, as in this case, Sahara sand.

Countersink
Countersink

More on applied products here

Further interesting applications from extremely diverse areas can be found here.


Go to manus® contest



Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH