Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Filling line for yogurt: Hygienically designed with plastic plain bearings

Manufacturer of filling systems, miromatic, uses the igus modular construction kit

Machines from miromatic fill containers with foodstuffs such as yoghurt fully automatically. The requirements regarding the hygiene and availability of the machines in such cases are high. The igus plain bearings made of high-performance plastics with incorporated lubricant prove their worth under these conditions.
In the Allgäu, the entire process chain of the food industry is at home – including machinery and plant construction. This chain begins with the well-fed cows of numerous farms and continues with renowned dairies and food processing companies. Moreover, renowned machinery and plant manufacturers based in the region specialise in the processing, filling and packaging of foodstuffs, with a focus on dairy products.

Profile

  • What was needed: iglidur J bearing bushings, drylin R linear round guides, igubal spherical bearings, iglidur J plain bearings, energy chains
  • Requirements: High availability in 24/7 operation, very high hygiene requirements, resistance to at least daily cleaning (aggressive cleaning agents, superheated steam, high pressure), lubrication-free, FDA approval
  • Industry: Beverages sector, bottling plants
  • Success for the customer: Our bearings are maintenance-free and wear-free. There are also polymer materials that have been specially developed for food processing machinery and have the appropriate approvals. For these reasons, miromatic design engineers have been using a wide range of our plain bearings for more than ten years.
miromatic filling system

Problem

Michael Rothdach GmbH in the Allgäu region of Germany is a renowned machine and plant manufacturer specialising in the processing, filling and packaging of food products - with a focus on dairy products. Under the brand name miromatic, the European market leader develops mixing systems for fruit yoghurt as well as bucket filling systems for food products such as yoghurt, mustard, ketchup and sauces. The filling plants are individually configured on the basis of the customer requirements, whereby the designers can resort to a modular system of individual standard stations. There are, for example, functional units for the process steps such as provision of empty containers, filling process (with weighing or inline flow measurement), lid supply and separation, lidding, sealing and labelling. All these modules vary and are therefore linked according to customer requirements.
Developers have to meet high availability requirements for all systems. A 24/7 operation is the rule rather than the exception. In addition, very strict hygiene requirements apply. Dairy products are very critical in this regard. That is why miromatic has developed various hygiene and sterile concepts, such as a line for the aseptic filling of dairy products under sterile air blanketing. All systems are designed to withstand at least daily cleaning with the usual methods (more or less aggressive cleaning agents, superheated steam, high pressure). In addition, the exposed drive elements are lubrication-free to prevent contamination, and the components and materials used are FDA-approved.

Solution

The plain bearings made of high-performance polymers perfectly fulfil this requirement profile. They are maintenance-free and wear-free and form a good friction pairing with aluminium and stainless steel. Approved polymer materials have also been developed specifically for food machinery construction. For these reasons, miromatic designers use a wide range of our plain bearings, and have done so for more than ten years.
Here are some examples: bearing bushes made of iglidur ensure precise guidance of rotary and linear movements on various guiding and adjusting elements (see picture 1 below). Depending on the application, housing bearings, such as the drylin R linear round guide here, are also used and simplify both production and assembly (picture 2). In ball screws, igubal spherical bearings compensate for misalignments (pictures 3 and 4). And the easy-to-use format adjustment at the sealing stations is implemented with iglidur J plain bearings (picture 5). Last but not least, our energy chains are also used, which supply energy and signals to the moving axes of the mixing and filling systems (also picture 5).
The material used from the iglidur range is decided according to the application. Apart from the "all-rounder" iglidur J, however, the bearings also have to meet special requirements for temperature, resistance to cleaning media or moisture absorption. There are special iglidur polymers for this.

iglidur bearing bushings in container separation Picture 1: Container sorting – iglidur J bearing bushes ensure precise guidance in the linear stroke.
drylin R linear round guide in lid sorting Picture 2: The lid sorting is implemented by drylin R linear guides. These pillow blocks consist of two parts and simplify the installation of the systems.
igubal spherical bearing lead screw Picture 3: Lead screws are mounted in igubal spherical bearings to compensate for misalignments.
Lead screws igubal spherical bearings Picture 4: Detailed view of igubal spherical bearing as support for the lead screws
Height adjustment of the filling station with iglidur J plain bearings Picture 5: The height adjustment of the filling station is implemented in the vertical linear stroke with iglidur J plain bearings. One of our plastic energy chains ensures safe cable guidance.

Here, you can find the products used

Here you can find further interesting applications from very different areas of use



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH