Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Single cores as energy supply

Single core cables from igus are used in EMAG's high-performance lathe centres

The vertical EMAG VMC lathe centres are also available as "five-axis machines" that enable the machining of complex geometries. For example, they make spatially inclined drill holes and surfaces in heavy components. This is a challenge for the energy supply to the spindle. EMAG relies on single core cables from igus' chainflex range.

Profile

  • What was needed: chainflex cables CF270 "spindle cables", energy chains
  • Requirements: Power of 84 kW and currents up to 252 A, hardly any installation space and good oil resistance
  • Industry: Mechanical engineering, vertical processing machines
  • Success for the customer: High saving of installation space with simultaneous cost reduction
EMAG VMC with CF spindle cable The VMC 450-5 MT enables high-precision five-axis machining of heavy components in a compact space.

Problem

High-precision vertical machining in five axes in a compact space: with this concept EMAG achieved real success in the precision machining market three years ago. The VMC 450-5 MT presented at that time is suitable for the machining of heavy components with diameters of up to 700 mm, which may also have inclined holes and surfaces. This is made possible by extending the basic model VMC 450 MT by a swivel axis (B axis) with integrated turning/milling spindle and a Y axis with integrated main spindle. The advantage: Manufacturers of gearbox parts and housings for lorries or mobile machines, for example, need a maximum of two machines instead of four or six, as was previously the case, to process a complete component. This saves space, costs and shortens the process chain.
Another advantage that applies to all vertical processing machines is their flexibility. The axes, shafts and housings are usually produced in medium quantities and with great variance. Set-up time is thus a crucial issue. Loading and unloading can be done by robot or manually. Optionally, the user can order an integrated tool magazine with up to 80 tools.
In the course of the development of the VMC 450-5 MT, the electrical designers also had the difficult task of supplying the high-performance spindle developed in-house with power and signals. The spindle motor has an output of 84 kW, there is hardly any space for the cables and during the acceleration processes currents of up to 252 A are achieved.
In addition, on vertical lathes the spindle is located below the workpiece and tool. The moving cables must therefore be well protected against swarf and oil.
Finally, the spindle cable must also be exceptionally resilient and of high quality. For example, the failure of a motor cable means that a replacement has to take place, which would mean a whole day of downtime due to the very compact design.

Solution

Under these conditions it was a logical step to implement the energy supply to the spindle exclusively with single cores.  The logic of this decision becomes even clearer when the alternative - a four-core motor cable with a cross section of 4G10 mm2 - is considered. Such a cable cannot be laid in the existing installation space, and its bend radius would also be too large.
However, there are reservations in electrical engineering about this type of energy supply, because the cores or cables can influence each other. The cables from the CF270 series of the chainflex range from igus were developed precisely for this application and for moving applications. They achieve extremely long service life, which is of great importance to EMAG and the users of EMAG machines. Since costs always play a role in machine tool construction, igus has adopted the principle of single-core cables from crane construction, while also reducing costs.
The result: The chainflex CF270.UL.D with PUR jacket, which is now known as a "spindle cable" in the market. It is, among other things, oil-resistant and notch-resistant, which is a great advantage in the oily environment of a machine tool with its many metal edges. The UL approval for the world market is of course also available here and this cable type can also convince in terms of price.
In the VMC machines, EMAG uses the single-core cables of up to a cross-section of 50 mm2, in special cases up to 70 mm2. The choice of material also contributes to this. The outer jacket is made of high-quality PUR. TPE is used for the core insulation below the shielding. This enables us to increase the temperature resistance of the cable, which takes into account the permanent high load on highly dynamic spindles.

"If a motor cable fails and has to be replaced, this means one day of downtime due to the very compact design. This is why a high-quality and resilient spindle cable is an important design feature."
 
Markus Pannicke, Lead Engineer Cable and Director at EMAG Leipzig
chainflex cables Multi-core cable (top) or single cores (bottom)? For EMAG there are good reasons to rely on single cores.
Cable single cores The non-moving cables of the USC machines are also designed as single cores.

Security thanks to guarantee and service life calculation

Based on more than 25 years of practical experience and also thanks to countless tests in the 3,800 m² test laboratory in Cologne, igus has been the only manufacturer on the market to give a guarantee of 36 months, or up to 40 million double strokes, on its chainflex cable range for over five years. In addition, the expected service life of the chainflex cables beyond the guarantee can be calculated using the online service life calculator. In EMAG's case the solution with the spindle cable CF270.UL.D means a high saving of installation space whilst at the same time reducing costs. Completely without risk for EMAG thanks to igus' comprehensive and resilient guarantee.
chainflex cables in the control cabinet View into the control cabinet. Clearly visible: the orange chainflex cables CF270.UL.D.
energy chain igus energy chains are used on several axes of the VMC lathe centres.



Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH