Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Reliable energy supply system in a gear grinder in a tight installation space

Plastic energy chains have been used in machine series for years without any problems

Realising a vertical lifting of over one metre and a pivoting range of 270° in a confined installation space was made possible in this application in the grinding head of a gear grinder. A conventional hanging installation of an energy chain was impossible, instead an e-chain with the fixed point mounted below was chosen. The e-chain, which can be moved from both sides, is directed over a guide roller and constantly tensioned.

Profile

  • What was needed: Energy chain systems from igus
  • Requirements: Particularly small installation space, pivoting range of the grinding head of 270°.
  • Industry: Machine tool manufacturing
  • Success for the customer: Special solution of the energy chain with pivoting guide roller to keep chain under tension
Discover all products for machine tools
energy chain The chain, which can move on both sides, is guided by a pivoting guide roller, which is connected to a counterweight by means of a toothed belt. This way the chain is always kept under tension.
Höfler Maschinenbau GmbH (now under Klingelnberg AG), a traditional company based in Ettlingen in Baden-Württemberg, specialises in the design of gear grinding and gear milling machines. For such a gear grinding machine, a special solution for the energy supply system had to be found for a customer due to the structural environmental conditions.  A vertical stroke of 1320 mm and a pivoting range of the grinding head of 270° (-180° to +90°) had to be achieved in a rather limited installation space. An energy chain in a conventional hanging arrangement could not be accommodated in the given installation space.
In order to meet the specified requirements, the energy chain system from igus was chosen as the fixed point at the bottom. The chain, which can move on both sides, is guided by a pivoting guide roller, which is connected to a counterweight by means of a toothed belt. This keeps the chain under tension at all times. In the meantime, the decision was made to install the energy chain in batch production due to the good experiences. The igus energy supply system has been used here for many years without any problems.
Catene portacavi
energy chain An pivoting guide roller safely guides the energy chain. An energy chain in a conventional hanging arrangement, on the other hand, could not be accommodated in the given installation space.
energy chain Rear view of the gear grinding machine. The energy chains and the guide roller disappear under the cladding.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH