Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
For the ValuTec milling machine, Waldrich Coburg is using pre-assembled readychain energy supply systems from igus. In addition to the energy chain, Waldrich also includes the chainflex single cables and the guide troughs in which the energy supply systems travel.
The energy supply system used in the milling machine consists of more than 8,000 individual parts, which had to be assembled at the right time and delivered on schedule. igus took over the procurement of all the necessary individual parts for the customer, right up to the delivery of the ready-to-install energy supply system. This made the costs transparent for Waldrich Coburg.
Whereas the machine builder previously had one supplier for each individual part, the chain, the cables and the hose systems with the corresponding logistical effort, Waldrich Coburg gets everything from a single source with pre-assembled readychain energy supply systems - straight from the manufacturer. Another advantage is the single point of contact at igus instead of many different contacts to deal with when such a large project is implemented. The system responsibility lies entirely with igus.
Dal lunedì al giovedì, dalle 8:00 alle 17:00.Venerdì dalle 8:00 alle 16:30
24h