Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Lubrication-free linear bearings in calf supports for cars and trains

drylin W linear bearings enable the maintenance-free extendable lower leg supports

An innovative lower leg support is designed to make long journeys in the car or on the train more comfortable: drylin W single and double rails are installed for the lower seat module's linear movement. The polymer bearings are lubricant-free, light, silent and insensitive to corrosion.

Profile

  • What was needed: drylin W single and double rails
  • Requirements: Lightweight bearing technology that operates silently and reliably in the application without lubrication or maintenance
  • Industry: Automotive industry
  • Success for the customer: drylin linear bearings are not only very lightweight, but also require no lubrication or maintenance, they generate minimal friction and no noise
Vehicle seat

Problem

This calf support is used in seats on trains or in cars where long journeys are to be made more comfortable. Linear rail technology guides the linear movement of the seat modification. Initially, at the development phase of this application, the company opted for LM ball bearings and shafts for use in trains but these had to be lubricated and maintained regularly. Since this maintenance was not always performed, functionality was limited. Other problems were the noise when the support was moved. This is not desirable in these particular applications. The previous solution was also simply too heavy for the area of application.

Solution

The customer was looking for a solution that would eliminate the disadvantages of the old solution and they found what they were looking for in our plastic bearings. Several rail systems were installed for calf support linear movement. Today, drylin W single rails and drylin W double rails are used (two WS-10 rails and four WJ200UM-01-10 carriages per calf support).
The advantage of the new polymer bearings in the application are that the systems are not only very lightweight, but also require no lubrication, therefore are completely maintenance-free. This also prevents mechanical failures. And the bearings generate hardly any friction and no noise.

Here you can find further interesting applications from very different areas of use:

Go to manus® competition



Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH