Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.
Les matériaux iglidur® sont d'excellents polymères, améliorés par des fibres de liaison en parfaite adéquation avec des lubrifiants solides, testés des milliers de fois et éprouvés des millions de fois.
Chaque année, les ingénieurs igus® mettent au point plus de cents nouveaux composites et réalisent plus de 3.500 essais sur des Paliers Lisses Polymères. Ils ont ainsi établi, au cours des dernières années, une vaste base de données sur les propriétés tribologiques des polymères.
Küppersbusch GmbH manufactures customer-specific beverage filling systems with igus® bearing technology.
Plain and linear bearings from igus® in multihead weighers
Les paliers lisses igus® font leurs preuves sur les parcours accidentés pour VTT.
In the new touring ski boot from Atomic, iglidur® plain bearings of the iglidur® J type in a white GLW collar bushing ensure the necessary mobility.
In the fitting systems of WSS, guide bushings and collar bushings made of highly robust iglidur® materials with incorporated lubricant are used.
3D printers: Linear components from igus® make production fast and resilient
This year’s Gold award winner is a system that assists doctors with keyhole cochlea implant surgery to treat inner ear deafness and profound deafness.
The winner of this year’s Silver manus® award is a machine that makes it easier to draw off screed.
This year, Bronze goes to a laser-based 3D printing machine that prints metal parts made of titanium, aluminium, steel or even gold.
This turbine is used wherever power is used but no mains connection is available.
This binding is used on so-called splitboards.
This crane crab runs on a reconditioned crane girder.
This bicycle frame was developed as a bachelor thesis at Aachen University.
This machine is used to split tree trunks.
This handling and contacting module is used for the automatic electrical measurement of individual boards in the temperature testing cabinet.
This centrifugal clutch is used in 2-stroke racing machines.
This corkscrew uncorks wine bottles automatically.
This wire-cutting machine cuts pipes for the oil and gas industry.
This 3D printer was constructed with almost no ready-made components.
This steering mechanism is used in a racing car.
This automatic packing station packs labels in boxes.
This robot is called “Porton Man” and tests protective clothing for the British military.
This robot checks the weld seams on pipes.
This isolator is used for the sterile packaging of syringes.
This column is used to store hoses or cables without twisting.
This racing car can be used both on a race track or as a rallye vehicle.
This device supports the levelling of dry fill material.
This device cuts figures and elements out of polystyrene blocks.
This washing machine is used in vehicle production.
This mobile robot is used during rescue operations following serious catastrophes such as earthquakes and bomb or gas explosions.
This stretching machine allows 50 percent of raw material to be saved with film/foil products.
and the first one that is variably adjustable in its width.
The drive power of this Segway similar vehicle is directly transmitted to the wheels.
The cinema seat can be optimally positioned for spectators.
This motor robot allows providing audio- and video information also under conditions that are hazardous to health and dangerous to life.
This machine decorates cakes.
These robots have an excellent grip.
This chair can be used to sit older or weaker persons up again after a fall without a great deal of strength being necessary.
This monoski permits disabled or people with reduced mobility to ski.
This system creates waves in public and private swimming pools.
This drilling machine is mounted on a trailer and is used to drill holes into concrete or asphalt.
This binding for skiers is lightweight and stable at the same time.
This motorcycle is usually to be found driving off the beaten track.
Lubrication-free plastic bearings for ergonomic office chair
Solar energy in continuous (dry-running) mode
These sunscreen slats are supported by maintenance and lubricant-free igus® iglidur® J plain bearings.
Clean, durable, and maintenance-free: polymer plain bearings in the food industry.
iglidur® bushings guarantee clearance-free and low friction motions in RC model racing applications
Pivot and rotate with plastic plain bearings - lubricant-free designer furniture with iglidur®
Maintenance-free polymer plain bearings for rugged mounted sweepers
Root ball transplanters are indispensable tools for tree nurseries and for garden and landscaping businesses.
In this case, the use of igus® products is not only advantageous from a technical, but also from a financial point of view when compared to competitive products.
Un constructeur de machines destinées à la production de pinceaux techniques, de renommée mondiale, fait appel à des paliers lisses de la gamme igus®.
Plastic plain bearings in process engineering: Completely maintenance and lubricant-free.
Due to their low weight, iglidur® Q plain bearings were used in place of bronze bushings for the spring suspension of the racing car.
Full-suspension mountain bikes use durable iglidur plain bearings.
Hinges for heavy doors in mega yachts: fully maintenance-free.
Seawater-resistant, wear-resistant polymer plain bearings are used in the new generation models of yacht building instead of self-made roller bearings.
Due to the excellent wear resistance and freedom from lubrication, iglidur® X6 bearings are used in wafer baking tongs.
Golfcraft golf trolleys made of carbon and aluminum - lightweight and foldable.
Stairs are no obstacle for this wheelchair.
The driver lies on this vehicle with his armed stretched out and head facing forward.
In this car-trailer, an igus® flange bearing made of iglidur® Z replaces the previously used phosphor bronze bearing.
igus® bearings are used for the gear shift linkage.
igus® plastic plain bearings are used here in the shock absorber of an excavator seat.
Moisture and extreme temperature fluctuations often lead to undesirable expansion of the component parts.
Plain bearings are used, made of iglidur® A500, an FDA-compliant high-temperature material.
This device is used for folding letters. The folding operation in a small space reduces the frame sizes of folding machines.
This machine can scan books fully automatically, with no human intervention required.
The components used must be suitable for use with food, which is why the design engineers decided in favour of xiros® ball bearings.
These fully functional steam locomotives have been built to a scale of 1:11.
This machining results in lost of wood chips and dust, of course, which would stick to lubricants.
This design was first used to deal with problems of clearance and friction. With iglidur® G plain bearings, however, these problems were eliminated.
A media-resistant bearing for small installation spaces was made from iglidur® bar stock.
Lightweight components are particularly important here to ensure as little energy as possible is required for movement.
Plain bearings from igus® are used for the movement of the front and rear wheels. Thanks to them, there are no problems with wear or corrosion.
This electric wheelchair also makes use of the properties of igus® plain bearings.
The bicycle pedal presented here responds to the ergonomic and biomechanical needs of cyclists.
Here, igus® plastic plain bearings have replaced classical roller bearings and stand up to environmental influences such as dirt and corrosion.
Silver Award at manus® 2011: String trimmer-cutting disc of PRODULEX UNIPESSOAL LDA, Portugal
This valve is used for filling ice-cream containing pieces of fruit in fully automatic industrial packing machines.
This small vehicle adheres firmly to surfaces with its magnetic wheels, to inspect welding joints.
This manus® contribution also shows an exceptional off-road wheelchair, the "Quadrix".
In this prosthesis for pneumatic knee joints, iglidur® J piston rings replace the previously used PTFE guide bands.
This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.
With this hand tool for the rolling and repairing of threads, the bearing support of the profi led roller is particularly important.
This manus® contribution is concerned with the cost-effective increase in production and process reliability for manual assembly using low-cost automation.
The bearings machined from iglidur® J bar stock are corrosion-resistant and have a low wear rate.
Fishing with a difference: with this harpoon you can hunt fish under water.
This high-pressure washer uses a planetary gear box.
This machine is used to pack products in blister film.
A conventional material in an unusual application: This bike frame is entirely made of wood.
Here, the honey is being loosened from the combs. For this, the honeycombs are pierced with needles.
This solar system can be installed either on its own or in combination with a wind turbine.
This information board is exposed to the weather and the forces of nature all year round.
This inspection robot was developed especially for use in pipelines.
By using iglidur® W300 plain bearings, reliability can be increased. The previously used ball bearings had to be oiled regularly, which is not the case with iglidur® bearings.
Since temperatures of several hundred degrees Celsius occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures.
Another newly developed dolly for camera movement is the subject of this manus® contribution.
This folding trailer “Tyligo” is extremely flexible and can be used to transport all kinds of things.
Provides a seat without taking too much room away from pedestrians: this is possible with the „Sitty“ folding seat.
To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.
xiros® polymer ball bearings were used for the rotary movements of the headrest.
This machine is used for preparing and drying kitchen herbs.
The various work processes like aluminum etching are sometimes done with extremely aggressive materials.
The high stressing through the three-shift operation and the shocks caused by the moving parts were crucial for the application of igus® products.
The main concern when designing the bearing support for this record player turntable was silent and low-vibration movement.
This laptop holder has been specially designed for hospital beds.
This walking aid has been built for children with brittle bone disease.
The exact positioning is important here, which is ensured by the combination of several igus® products.
This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.
This doll is used for representing maritime signals and originated from a marketing project in collaboration with a doll builder.
This pagepulltester is a high-precision measuring instrument for the bookbinding industry.
This fully functional hydraulic excavator was copied on a scale of 1:14.5.
Model train enthusiasts will enjoy this Rhätische Railway locomotive for a long time to come.
The stones used can weigh anything up to 4,000 kilogrammes. This means a heavy-duty load for all the components used.
This solar thermal power plant also obtains energy from the rays of the sun, without fossil fuels.
The manus® contribution submitted here is the new development of a patient lift for ambulances for transporting patients who are able to sit in the vehicle.
In this application, metallic ball bearings and DU bushings have been replaced by lighter iglidur® flange bearings.
xiros® ball bearings from igus® are used in this planetary gearbox that is used in wind turbines.
This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.
This machine is used for loading and unloading of boxes at an automated warehouse.
The suspension pins in this racing car were previously guided without bearings.
An extremely light weight is the most important criterion when constructing a racing bike brake.
This robot arm is so strong that it can use a drill.
This contribution to the manus® competition – a robot gripper – is extremely flexible.
Special Award at manus® 2011: Robot Head of Archimedes Solutions GmbH, Germany
With this application, salami is cut into slices. As with all applications in contact with food, here too lubricants cannot be used.
Here, sanitary elements in the bathroom unit are installed with igus® products.
This machine weaves and prints terry cloth hand towels.
This machine is also used for processing food, in this case raw ham.
All igus® products used are maintenance- free, giving the machine a long service-life.
The „ConCut“ is a CNC-controlled cutting system for confectionary products.
A tarp is lowered slowly over the car, so that at first only the outlines are visible; then the tarp is cut by the special mechanism and the car is presented to the public.
This cutting mechanism is used in the beverage industry. Several igus® products were used here.
Children are especially prone to squeeze their fingers in glass swinging doors. This safety door prevents that, because it „gives“.
This innovative sledge allows people to ski sitting down. The sledge is steered by the feet and tilted by the hands.
This exceptional sporting equipment makes bombing down a ski slope like riding a bicycle.
This device can help ski jumpers to improve their jumps.
iglidur® plain bearings and thrust washers are shown here in the service of art.
This solar system can be installed either on its own or in combination with a wind turbine.
For solar systems to retain their entire performance capacity, they have to be cleaned at regular intervals, particularly in sandy regions.
Previously, metal bearings and linear guides were used, which rusted quickly and therefore required frequent maintenance.
No matter how much the sun shines: these sunshades ensure pleasant light conditions within the building.
This special wheelchair allows people who can only walk with diffi culty to go to the beach.
This motor is to drive deep-sea robots even at 6,000 metres under the sea.
Gold Award at manus® 2011: Machine for frying Spanish omelettes of Carmelo Lagunas Escudero, Spain
This equipment is used in the food industry. The baked goods are separated on these chains.
In this pedal boat, the moving parts of the drive mechanism must be mounted free of lubricants, since the screw is in the water.
This dry toilet has special requirements for the components used.
Dans cette application des paliers lisses en iglidur® Z remplacent un roulement à billes et un roulement à aiguilles dans un réducteur à renvoi d'angle
Seawater is a very corrosive environment on account of its high salt content. Components that are exposed to the water must withstand it.
This fully automatic page turner for people with disabilities can automatically turn the pages of many newspapers, magazines, folders, exercise books and the like.
This application shows a conversion kit for the suspension in three-wheeled motorcycles.
igus® thrust washers and flange bearings were used for the new design. They made the elaborate milling of the base plate unnecessary.
This equipment can package various industrial products, with any materials.
the armrests of this chair are adjustable, to accommodate the needs of the individual user.
This device uses wind power to generate electricity.
In this exercise equipment, vibrations are specifically used to build up muscles.
Any movement that is to be performed here must be lubrication-free, executed free of wear and, if wear does occur, it must be free of heavy metals, etc., that could give distorted results in the chemical analysis.
The use of iglidur® bearings quadrupled the service life of the machine. It made it possible to save almost 300 mechanic-hours plus ca. 8 tonnes of cotton wool.
For the gripper bracket for screws in automatic screwing devices – previously a job done by steel cheeks.
This application creates new possibilities in steel construction, shipbuilding, cable cars, plant engineering or in general mechanical engineering.
With this snowboard, the “Twistboard”, both parts are connected via an axially aligned joint.
Application of plastic plain bearings in an automatic welding plant.
Le prototype d'un "Chemical Accident Roboter" a été mis au point par quatre étudiants.
Passage à des paliers lisses polymères isolés, insensibles à la foudre et résistants à la corrosion sur tout l´avion.
The unusual design for a recumbent bicycle has got what it takes: cordless screwdrivers are used here to drive it.
Les paliers lisses économiques, légers et sans corrosion correspondent aux spécifications de cette application.
Pour le logement des essieux de machines agricoles, la charge de bord en particulier est souvent un critère décisif pour le choix des paliers.
Rheinische Fachhochschule Köln (institut technique supérieur de Cologne) : réduction de la friction lors de la sortie du bras à caméra du "ball gripper"
Paliers lisses polymères iglidur® dans des grues utilisées dans les ports de plaisance commerciaux et privés ainsi que par des propriétaires de bateaux afin de sortir les bateaux de l´eau.
Chemical-resistant and corrosion-free: maintenance-free polymer plain bearings in catering kitchen appliances.
Le faible encombrement et l´absence de corrosion des paliers lisses en iglidur® J ont été décisifs pour leur utilisation.
Vent, sable et soleil : Paliers lisses polymères dans la technique solaire
Les paliers lisses en iglidur® G doivent tenir face à des courses courtes linéaires et des angles de pivotement changeants accompagnés d´impacts variant eux aussi.
Les Paliers Lisses iglidur® G ont fait leurs preuves grâce à leur fonctionnement sans entretien ni lubrifiants, a leur excellente résistance à l'usure à fortes charges et leur bonne tenue aux agents chimiques.
Guidage et logement sans entretien des supports des bras et des repose-pieds d´un fauteuil de dialyse.
Des paliers lisses en iglidur® G ont été installés en 2001 et fonctionnent sans graisse et sans usure notable dans le milieu très rude des machines de construction.
Le fonctionnement entièrement à sec et l´insensibilité à la saleté qui lui est liée sont d´une grande importance en contact direct avec les produits à semer.
Compétition internationale de robots : L´Université technique de Chemnitz se compare à la concurrence internationale.
Des paliers lisses dans le secteur de l´emballage pour éviter frottement et usure.
Des paliers lisses polymères dans une atmosphère quasiment sans oxygène : Record du monde d´altitude en montgolfière.
Pivotement et rotation avec des paliers lisses polymères - Nouveau système à lamelles de verre / façade réglable du centre de services d´un constructeur automobile.
Les paliers lisses polymères sont de plus en plus présents dans la fabrication traditionnelle d´orgues.
Des frites de grande qualité - les paliers lisses polymères sans graisse de cet appareil de filtrage de la graisse de friture contribuent à maintenir la qualité à un niveau élevé.
Les Paliers Lisses iglidur® Q peuvent absorber de très fortes charges et faire face à différents angles de pivotement. C'est pour cela qu'ils sont la solution idéale pour la trottinette électrique "Zoob".
Toujours prêts - ... tout en restant économiques. Les paliers lisses évitent les temps d´arrêt, même à long terme.
Pivotement et rotation sous pression - polymères hautes performances dans l´usinage du bois.
Le choix des gagnants : Ce dérailleur de pointe bénéficie des qualités des paliers lisses polymères.
Le bien-être des patients comme objectif principal : Amélioration d´une prothèse articulée avec des paliers lisses polymères.
Les paliers lisses polymères rendent le remplissage des bouteilles en PET plus économique.
Paliers lisses polymères dans la construction de machines-outils chez Deckel Maho Gildemeister.
Précis et durables : Paliers lisses polymères sur une nouvelle machine à refendre le cuir.
Pour une durée de vie plus longue - capteur d´angle à tout(s) prix avec palier spécial dans des presses d´impression.
Propreté requise : Les paliers lisses polymères fonctionnant sans graisse sont le produit idéal pour le secteur alimentaire et les spécifications hygiéniques sévères.
Contrôle d´usure : Les paliers lisses jouent leur rôle pour le contrôle de joints pneumatiques.
Des pièces spéciales compensant les tolérances dans le secteur rude de la construction de machines agricoles.
New solutions for fitness equipment save production costs and assembly times.
L'excellente résistance aux produits chimiques a joué un rôle décisif dans le choix des Paliers Lisses iglidur®.
Palier lisse iglidur® G dans le vérin hydraulique d´une machine de construction.
igus® goes to Hollywood - polymer plain bearings in a camera jib
Les réductions importantes du poids représentent un avantage essentiel en sport automobile. Un avantage dont disposent les paliers lisses en iglidur® W300.
On the ecoflow pumps, "iglidur® X" plain bearings of various sizes are used.
L´insensibilité aux charges de bord est importante sur cette application, en plus de l´absence totale de graisse et d´entretien.
Les modules à DEL pivotent à l´aide de moteurs et de paliers iglidur® JVFM-0810-08.
Les paliers lisses en iglidur® J se distinguent par une absence totale d´entretien dans les milieux très sales.
Stabilisation du train de roulement des robots sans perte de flexibilité avec des paliers lisses igus®.
Les paliers lisses iglidur® G se distinguent par une grande résistance à l´usure et un fonctionnement totalement à sec sur cette machine d´emballage de chiffons à polir.
En plus de leur grande résistance aux produits chimiques, les paliers lisses en iglidur® J permettent à cette application de fonctionner véritablement à sec.
En plus de leur grande résistance aux produits chimiques, les paliers lisses en iglidur® J permettent à cette application de fonctionner véritablement à sec.
Sur cette application, des paliers lisses iglidur® J ont remplacé les roulements à billes graissés.
L´utilisation de paliers lisses iglidur® RN a permis de réduire considérablement la force motrice nécessaire pour des installations de lavage de bouteilles.
Une très grande résistance aux produits chimiques et la possibilité d´avoir de petites quantités ont été décisives pour le choix des paliers lisses en iglidur® X pour presque tous les robinets à boisseau sphérique de la société Pister.
En service continu, les poutre de scellement des ensacheuses atteignent souvent des températures de 160 °C et plus.
Des palliers polymères sans entretien sont utilisés dans les chaînes à rouleaux assurant l´entraînement des groupes principaux ou auxiliaires.
La grande résistance aux charges de bord est la principale raison qui a conduit à l´utilisation de rondelles en iglidur® G.
Quick, straight, precise: this is how the requirements in sheet metal machining can be summarized. Sophisticated straightening technology makes all this possible.
iglidur® propose des améliorations à plusieurs niveaux pour les rickshaws.
Les paliers lisses iglidur® Z utilisés dans le grand huit du parc à thème Six Flags ont entraîné une réduction nette des coûts.
L´absence de corrosion est un argument important pour l´utilisation des paliers lisses en iglidur® G dans la robinetterie de bateaux.
Ce sont surtout la résistance élevée à l´usure et l´absence d´entretien qui ont motivé le choix des paliers lisses iglidur®.
Seule l´utilisation de paliers lisses en polymères a pu garantir une utilisation sans huile du moteur.
L´iglidur® G est idéal pour cette application en raison de son absence de graisse et de sa résistance à la corrosion.
Sans graisse et silencieux : iglidur® G dans une table thérapeutique
Les paliers lisses en iglidur® D se distinguent par un très grand avantage en terme de coûts par rapport aux douilles métalliques roulées courantes ainsi que par une grande résistance à l´usure.
Toujours dans le mille – des Paliers Lisses Polymères pour de jeunes ingénieurs de l'Université technique de Munich.
Multi-step, single-flow underwater motor pumps with integrated non-return valve.
Une réduction de moitié de la force motrice nécessaire à ces laveuses de bouteilles a été l´un des résultats de l´utilisation de paliers lisses iglidur® RN.
Ecole d'enseignement professionnel de Burgdorf-Lehrte : passage d'une transmission à engrenages à un entraînement à courroie crantée sur un robot existant.
Tribo-polymères sans graisse dans une application extrême - installation d´emballage de profilés.
Un oeuf sur quatre roues : Des embouts à rotule et des paliers lisses polymères assurent la mobilité de ce véhicule à hydrogène.
Des embouts à rotule et des rotules lisses robustes, insensibles à la saleté et sans entretien sont utilisés dans des véhicules communaux spéciaux.
Utilisation de paliers lisses polymères dans une machine de fabrication de noyaux.
Trophée de bronze pour le Manus® 2007 : traitement de produits en vrac
Trophée d'or pour le Manus® 2007 : machine à refendre "Autosplit-D3"
manus® d´argent 2007 : Body-Spider® de la société KOOPERA GmbH
Maintenance-free track accuracy
Lifting heavy loads
No more expensive repairs
Low vibration in the wind
No lubricants in food sector
Resilient and TÜV-tested
Precise and ergonomic
For wind and rain
Hot and quick
secure guidance
Robust under high forces
Long-lasting and cost-effective
Very resilient
Harsh surroundings and dirt
The used bearing must be lubricant-free, because silica sand is used here.
The plain bearing used has a low frictional resistance and is low maintenance and lubricant-free.
Quick and light
Can be handled alone
Simple movement
Maintenance-free dosing
Reliable and cheaper
Easy and durable
Léger et sans jeu
Quiet and maintenance-free
Robustesse et réduction des vibrations
Precise and effective
Saves costs and better
To victory with igus® - maintenance of the suspension fork eliminated.
Less wear
Hot and cold
En eau de mer sans corrosion
Affordable and long-lasting
Wear-resistant and secure
Robust and light
Capacité de charge élevée et longue durée de vie
Robustesse et réduction des vibrations
Cost-effective and maintenance-free
Economical even when exposed to heat
Simple but robust
High positioning accuracy
Quiet and low friction
Maintenance-free and resilient
Light and reliable
Resistant and long-lasting:
Over 170,000 Euro of benefits were able to be achieved by using polymer plain bearings
Secure under high forces: maintenance-free plain bearings made of iglidur® Z can withstand extreme loads.
Capteur d´angle économique avec palier spécial dans des machines d´imprimerie.
Sur les solutions conventionnelles, les produits de nettoyage lavaient la graisse des paliers et poussaient même parfois de la saleté dans les paliers.
Les roulements à billes traditionnels ont été remplacés par des paliers lisses polymère iglidur® dans un nouveau mécanisme.
Utilisation systématique de paliers lisses igus® dans la structure de l´avion réalisé
en construction sandwich alvéolaire à fibres composites.
Cette chaise de bureau tournante s´adapte automatiquement au poids de son occupant.
Tête d´application d´un distributeur de poignées.
Augmentation de la durée de vie, de la fiabilité de la machine, de la solidité et de la capacité de charge grâce à l'emploi de Paliers iglidur® dans les galets de roulement de cette mini pelleteuse.
Plus de 30 paliers lisses polymères iglidur® contribuent à remplir les spécifications.
La direction de ce chariot de manutention a été revue et fait appel à des paliers lisses polymères igus®.
Les matériaux pour paliers qui se distinguent par des qualités telles qu´un faible frottement à sec, une bonne résistance aux produits chimiques.
Plan de travail réglable pour postes de travails pour personnes handicapées.
Le problème à résoudre lors de l´étude résidait dans le manque de place en raison de la combinaison de deux mouvements indépendants l´un de l´autre et de la sollicitation mécanique élevée.
Ce support fait appel à un plateau tournant en polymères iglidur® qui se distingue par son faible poids.
Le poids d´ensemble et les forces de levier générées posaient problème aux concepteurs. Le poids devait absolument être réduit.
Montage très simple malgré les paliers lisses.
Ce prérégleur d´outils fait appel à des chariots de guidage drylin® en iglidur® J200 pour la mesure. Ils contribuent à la précision de l´application et à unereproductibilité de+/- 0,1mm.
Jointeuse de placages
ACR-Speedstar : Des économies grâce aux paliers lisses polymères.
iglidur® G résout les problèmes sur cette tête de rotor. Les lames du rotor tournent environ 400 fois par minute avec un angle de mouvement maximal de 30°.
Agitateur utilisé dans des agents liquides dans des installations de méthanisation.
Dérailleur pour VTT (or olympique2004).
Des réflecteurs à UV inchangés depuis 10 ans ont été repensés et certans détails améliorés. Des paliers appliques en iglidur® Z y réduisent les coûts et les besoins en entretien.
Cette chaîne a été optimisée pour répondre aux besoins du marché grâce à un logement quasiment sans usure qui résiste en même temps à une pression élevée.
Le vérin est totalement sans entretien grâce aux paliers lisses iglidur® et le poids a pu être réduit à environ 10% de celui de la solution d´origine.
Le joint de Cardan présenté ici se distingue des joints courants dans la mesure où il n´a pas été conçu seulement pour la transmission de torsions.
La mobilité de la main robotique est assurée par près de 99 Paliers.
Le réglage du dossier est assuré avec des produits drylin®, les appuis-tête sont guidés dans le dossier avec des paliers lisses polymères en iglidur® G.
De l´iglidur® X a été choisi pour les paliers lisses destinés au guidage de la tige de piston en raison de sa résistance aux températures élevées et de sa résistance suffisante à l´humidité.
Les charnières et les roulettes des rampes sont chacune équipées de deux paliers lisses en iglidur® Z.
Le mouvement des registres d´une orgue doit se faire avec le moins de bruit et de frottement possible.
Nous avons cherché un palier capable de résister à l'huile chaude jusqu'à 220°C et pouvant être au contact d'aliments. La solution au problème : l'iglidur® A500
Le challenge au niveau de l´étude résidait dans le fait que le logement du module devait être conçu pour une utilisation dans l´eau.
Des paliers lisses igus® vont être utilisés pour la série afin de répondre aux besoins très variés du logement.
La disponibilité de l´application, même à des températures supérieures à 100 °C, a été assurée à l´aide de paliers lisses polymères en iglidur® X.
Le passage d'une combinaison plastique-métal à une combinaison plastique-plastique pour les paliers a permis une mise en oeuvre intégrale.
Le nouveau système de transport de charges en extérieur par hélicoptère devait avoir un faible poids et une grande fiabilité tout en étant résistant aux intempéries et en n´exigeant aucun entretien.
Ce matériau meilleur permet de réduire les coûts d´encore 60%.
L´utilisation d´un nouveau design qui fait appel à un seul élément en polymère iglidur® RN56 comme pièce maîtresse a permis de remplir les spécifications techniques tout en réduisant nettement les coûts.
Contrôle de l´énergie et de torsion pour une jambe prothétique
La principale nouveauté au niveau de la conception résidait dans l´utilisation d´un palier lisse iglidur® à l´extérieur des tétons.
Même après une longue utilisation, aucune augmentation notable du jeu ni de l´abrasion n´a pu être constatée grâce à l´utilisation de paliers lisses igus®.
Un principe de fonctionnement modifié ainsi que l´utilisation de paliers lisses polymères ont permis de créer une nouvelle génération de disques sans entretien et plus économiques.
Fermeture automatique d´une capote de cabriolet: Le jeu axial maximum a pu être réduit de 1,5 mm pour passer à 0,5 mm grâce à l´utilisation d´un palier à collerette calibrable igus®.
La nouvelle disposition des paliers lisses a permis aux roues motrices du véhicule de transport d´utiliser la rotation de chaque palier lisse pour faire passer les roues avant par un poste de déchargement avec une trajectoire parfaite.
L´utilisation d´une combinaison de paliers en polymères à collerette élastique permettant un montage sans jeu du crochet de verrouillage a joué un rôle décisif pour le respect de toutes les spécifications.
Support de roue pour véhicules de tourisme : Ce système est utilisé depuis un an environ chez le client sur une base journalière et sans le moindre problème.
L'emploi des Paliers igus® dans cette application signifie aussi : une dispositif de qualité, un montage rapide, une très longue durée de vie (2 millions de cycles) et une robustesse hors pair.
Les paliers lisses sont en place depuis un an environ et fonctionnent sans problème pendant la production.
L´utilisation de paliers lisses iglidur® a permis de faire des économies au niveau du logement.
Lesroulements à billes posent de gros problèmes en raison de la graisse, notamment sous l´eau. Pour des raisons économiques, les versions en acier inoxydable n'ont pas été retenues dans cette application.
Les tolérances du palier ont pu être nettement améliorées grâce à l´intervention au niveau du diamètre intérieur du palier lisse polymère en iglidur® P.
L'emploi de Paliers Lisses polymères dans une machine pour câble pour pneu garantit la résistance au fluage.
L´utilisation de boîtiers linéaires drylin® et de paliers lisses en iglidur® G permettent au boulon de centrage d´avancer facilement et sans saleté.
Les paliers igus® semblaient d´autant mieux adaptés à l´application décrite qu´ils étaient résistants à l´eau, à la saleté et aux températures élevées en plus d´être sans entretien.
Principales exigences de cette application : grande précision dynamique, faible poids pour une grande rigidité et disponibilité élevée en service sur 3 postes.
igus® a créé une pièce moulée par injection qui a été placée dans la coque du boîtier et y fonctionne très bien depuis cinq ans déjà.
Equipements de contrôle de pièces frittées : Un guidage linéaire sans graisse (encrassement du liquide) doit être assuré.
Bras pivotant monté sur roulements à billes en polymères dans des machines de moulage par injection : La structure simple à enfichage et les bagues réglables ont permis de renoncer à un mécanisme à joint compliqué.
Plain, spherical and linear bearings made of plastic help to improve mobility and the quality of life
Previously used cables have been replaced by flexible CF9 TPE control cables, which have a significantly longer service life.
Exhaust valve on CNC drilling and milling machines
The suitability of iglidur® G plain bearings in pedal and lever bearing assemblies was proven in a test.
High, jerky loads are not a problem with plastic plain bearings.
Le « Mercruiser Six » a été conçu pour des bateaux de course à grande vitesse.
The plain bearings in the components are constantly exposed to air containing acid.
Replacement of metal bearings in concrete drilling and concrete sawing machines.
Dispositif de levage de moteur de bateau et enrouleur de mât équipés de paliers lisses polymères.
Complete freedom from maintenance and stick-slip-free movement are the prerequisites for use in office chairs.
Printer and plotter - low drive forces, low sliding friction coefficients.
The plain bearings must withstand static radial loads of 25 N/mm² at temperatures of 170°C - 200°C.
Clipless bike pedals for use on road bikes and for road racing.
Overhead conveyors for transporting packaged goods within the factory are used to transport a wide variety of goods.
The needle bearings previously used had to be serviced or replaced every few years.
Lubrication-free and wear-resistant bearings under extremely high load.
Widely different sliding speeds - no problem with polymer plain bearings.
iglidur® M250 plain bearings replace porous bearing bushings.
750,000 switching operations were required without failures.
Loads up to 2000 N at temperatures of up to 250 °C characterize this application.
In the extremely chemically aggressive environment of semi-conductor production, metal plain bearings were regularly replaced after 2 to 3 weeks. Using iglidur® X plain bearings, the bearing point could be operated for years without problems.
Low wear on a wooden chair thanks to iglidur® A200 flange bearings.
iglidur® G plain bearings of different sizes are used on this equipment.
These sensors are used to prevent the blocks on the individual cranes from moving.
In drilling and sowing machines, the plain bearings are exposed to extreme levels of dirt, weathering and shock loads.
Bearings on guide vanes in condensers.
Due to their lower weight and better suspension qualities, the company switched to igubal® rod end bearings.
Thanks to iglidur® plain bearings, the company was able to reduce its costs by 93%! The assembly times were reduced by 10 minutes.
Maintenance-free plastic plain bearings in a music box.
Suspension of a bearing compass.
Requirements: fluctuating ambient temperatures, use in steam pipes with steam temperatures of 135 °C, use in acid and alkali tanks.
Due to the aggressive paper dust, the sintered bearings used before clogged up very quickly.
Vibration caused by the rotating wheel had to be dampened and the bearing assembly had to be corrosion resistant in order to withstand strong fertilizers and dew dampness in the grass.
The iglidur® plain bearings are used here in various bearing points.
This roller table represents a possible iglidur® D application, where it is a matter of the lowest possible drive forces.
Various plastic plain bearings are used on the different articulated joints of this multifunctional wheelchair.
A wheelchair ramp with plastic plain bearings was designed and installed at the front entrance of a low-floor bus.
Compared to the metal plain bearings first used, the better vibration dampening of iglidur® X reduced the noise of the cutter head.
Physiologically safe bearing assembly in a medical hose pump.
The load on the bearing is around 10 N/mm², approx. 1000 cycles are performed per day.
The rolled plain bearings used before often used to fail due to wear.
Used in difficult conditions: vibration, random forces, sudden shocks and cold, wet snow.
Snowboard-like appliance
The plastic bearings used do not need any oil and remain functional and clean. The performance of the plastic is not affected by extreme temperature fluctuations (hot and dry, cold and wet).
The bearings in this chain conveyor must be able to run dry, yet also come into contact with aggressive coolants and metal powders.
Stop slide module on an automatic cake decorator.
A special size bearing was developed so that it fits into the existing bearing without hindering the wall thickness.
The system uses an electromagnetic drive (plunger coil), which enables the required air pressure to operate piston and cylinder.
iglidur® W300 plain bearings are used here as a replacement for recirculating ball bearings.
The baking ingredients can easily settle in the mixer's catch and make it stick. iglidur® J is made of plastic and is therefore resistant to dirt and chemicals.
The telemark bindings kept on breaking and failing. A sturdy, maintenance-free product was able to be achieved using the iglidur® plastic bearings.
Machine for producing sausage casings.
Paliers lisses polymères iglidur® dans des clapets d´admission d´air.
Paliers lisses polymères iglidur® dans un tendeur de courroie.
Paliers lisses polymères iglidur® dans les étriers de frein d´un véhicule utilitaire.
Paliers lisses polymères iglidur® dans une fusée d´essieu devéhicule utilitaire.
Paliers lisses polymères iglidur® dans des charnières de porte.
Paliers lisses polymères iglidur® dans une capote de cabriolet.
Paliers lisses polymères iglidur® dans un système de pédales.
Paliers lisses polymères iglidur® dans un siège de véhicule.
Paliers lisses polymères iglidur® dans la direction d´un véhicule utilitaire.
Paliers lisses polymères iglidur® dans des papillons des gaz.
Paliers lisses polymères iglidur® pour le logement d´une cabine de conducteur.
Afin de simplifier le processus de production et d'en réduire au maximum les coûts, il est essentiel d'utiliser un minimum de pièces différentes. Le compromis entre stabilité et flexibilité a pu être résolu à l´aide de paliers lisses iglidur® d´ igus®.
Le choix s´est porté sur les paliers lisses igus® parce qu´ils sont sans entretien, économiques et très faciles à utiliser.
Utilisation d´une table à vis hélicoïdale de grande qualité, de guidages linéaires et de rotules lisses igubal®.
Lors de la mise au point du grappin, l'accent a été mis sur la réalisation de mouvements simples, la légèreté de la construction ainsi que l'obtention du plus grand rayon d'action possible.
Ecrou pour vis trapézoïdale drylin® dans une machine d´usinage de tôle.
Polymère plutôt que circulation de billes - guidages linéaires drylin® pour l´ébavurage à la machine.
Paliers polymères sans entretien dans des scieries fixes et mobiles.
Des guidages linéaires drylin® rendent ces appareils de manipulation compacts tout en étant très flexibles.
Paliers drylin® en polymères dans un appareil d´inspection de tube prolongateur off-shore.
Une machine de gravure équipée de produits igus®, projet de fin d´études après une formation de quatre ans en automatisation.
Utilisation de paliers drylin® haute température pour le logement de la poutre de scellement d´une ensacheuse.
drylin® dans une boucheuse de bouteilles
de vin mousseux.
Using drylin® T linear guide and iglidur® PRT slewing ring bearings, the movement under the press and the pivoting of the parts to be assembled is mastered.
Leobot robot: Robot design for participation in the Eurobot competition.
Automatically aligning the photovoltaic tracking systems to the position of the sun with the aid of lubricant-free plastic plain bearings produces a particularly high efficiency.
Since the clamping stars in this bottling plant were equipped with polymer bearings, the service life has almost doubled.
On these horizontal forming, filling and sealing machines, the total freedom from maintenance over the machines' entire life cycle was particularly important for the customer.
Initiated by Sachs Bikes, Norbert Staffend started with a focus on "motorized two-wheeler" in the student project. The result was this pure and elegant e-scooter
The Shell Eco-Marathon is the largest energy-efficiency competition and is aimed at student teams from across Europe.
Rugged liquid manure tank trucks are used for the economic distribution of biogas manure. In the steered pendular axles, lubricant-free polymer bearings defy all adverse conditions.
Ce projet est un projet d'études visant la mise au point d'un modèle réduit d'avion. Des paliers lisses iglidur® ont été utilisés pour le logement de l'aileron.