Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Conveyor belts for people

A safety mechanism for person belt conveyors, also known as moving sidewalks, with high speed has been developed. The Norm DIN EN 15700 applies for this type of conveyor belt. To increase the speed from 0.7 m/s to 1.2 m/s, a new “safety exit” is necessary. It is located at the end of the drive station and must be designed in a way, that it is initiated at a maximum force of 50 N in the area of danger. The braking distance is 500mm. A safety zone has to be created for the passenger in order to not get injured. Different safety sensors are additionally used.  This kind of person belt conveyor is mainly used outside in the mountains. Because they are not only used in the wintertime, a safety exit needs to be guaranteed at all times. Different safety elements have been installed, among which plastic bearing materials made of iglidur® J are relevant: Low friction, high reliability, shock-proof, freedom from maintenance and suitable for temperatures from -25° C up to +40° C with dryness and humidity. First systems are already installed in France, and others all over Europe are planned or already under construction.
Conveyor belts for people

LST GmbH, Werner Rainer, Bad Tölz, Germany

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:

Go to manus® competition



Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® SE & Co. KG signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® SE & Co. KG