Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ? |
Due to customer request, igus harnesses all its cables with the appropriate connector in-house. With more than 4,200 drive cables available made in line with to 24 manufacturer standards, the customer always finds the most cost-effective cable for their a26.11.2018
If the user is looking for a highly flexible drive cable, then igus offers technically the best and the most cost-effective solution from more than 4200 cable types according to 24 manufacturer standards with the readycable product finder. Simply enter the part number of igus or the manufacturer, or select the name of the drive manufacturer from the menu. Then click on the required cable type and the product finder will list all suitable drive cables. The overview covers the various cable qualities, such as PUR, PVC or TPE outer jacket, including their most important properties such as bend radius and travel length. The newly integrated service life calculator predicts the lifetime of the cable in the e-chain after entering various parameters, such as speed, operating temperature and acceleration. The price is also displayed. With another click, the selected part can be added to the shopping cart. The chosen drive cable is delivered to the required length, with centimetre accuracy, and shipping starts from 24 hours. All this without surcharges, and from a quantity of one. |