La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
Presse |
|
Avete qualche richiesta? Avete bisogno di materiale? Le informazioni aggiornate per la stampa e il materiale fotografico pronto da pubblicare sono disponibili per il download qui. Contattateci telefonicamente, via e-mail o fax! |
|
Contatto stampaVolete essere aggiunti alla nostra lista di distribuzione per i media? |
Fast drive for a small price: New igus cable for SEW and Siemens motors26.11.2018
In order to drive motors, many engineers increasingly come face to face with hybrid cables. In these drive solutions, the energy supply and other functions run on a single cable. In this way, for example, the motor manufacturer Siemens replaces the encoder cable with a BUS element and adds this to the energy cores. This eliminates the need for cabling with a separate measuring system cable for the encoder. igus has now expanded its low-cost hybrid cable series with the CF280.UL.H, which is suitable for motors of SEW and Siemens. The new highly flexible cable is specifically designed for use in the energy chain. It is suitable for applications up to a bend radius of 10 x d across all industrial sectors from the machine tool and automotive industry up to intralogistics. Even temperatures from -25 degrees up to +80 degrees Celsius pose no problem for the cable. Depending on the manufacturer's specification, the new hybrid cable has a black or orange oil-resistant PUR outer jacket, is coolant-resistant and flame-retardant.
A braided shield with high coverage ensures good EMC protection of the cable over a long service life. igus regularly carries out continuous tests on all cable ranges in the world's largest laboratory spread across a floor area of 2,750 square metres. In a series of tests at 7.5 x d, hybrid cables survived over 8 million cycles without damage. Another advantage of the new cable series is that it has the American UL approval, as well as the EAC and CTP certificate for the Russian market. |