La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
Presse |
|
Avete qualche richiesta? Avete bisogno di materiale? Le informazioni aggiornate per la stampa e il materiale fotografico pronto da pubblicare sono disponibili per il download qui. Contattateci telefonicamente, via e-mail o fax! |
|
Contatto stampaVolete essere aggiunti alla nostra lista di distribuzione per i media? |
Cables for drive technology found, ordered and connectorised quickly at igus03.01.2019
If the user is looking for a drive cable, then igus, with its portfolio of more than 1,350 cables, always has the optimum solution for the respective application at the most cost-effective price. The motion cable specialist has been developing cables specifically for use in the energy chain for over 30 years and testing them in the largest laboratory for moving applications in the industry. With over two billion test cycles and more than 1.4 million electrical tests per year, igus is the number one for moving cables in energy chains. The new website www.igus.eu/drive now provides a new gateway to the diverse world of igus cables. From cables sold by the metre and the harnessed, ready-to-connect drive cable with connector up to the special cable in the desired length. The customer has a wide choice. The "Drive" website offers the user a comprehensive overview of the drive technology, the igus test laboratory and the in-house harnessing of cables. In addition, the user has the option to order free samples or directly order the appropriate cable that he wants from the shop. |