La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
Presse |
|
Avete qualche richiesta? Avete bisogno di materiale? Le informazioni aggiornate per la stampa e il materiale fotografico pronto da pubblicare sono disponibili per il download qui. Contattateci telefonicamente, via e-mail o fax! |
|
Contatto stampaVolete essere aggiunti alla nostra lista di distribuzione per i media? |
e-chain expert: ready-to-connect energy supply system easily configured online09.06.2019
The quick way to a ready-to-connect energy chain is made even easier with the igus e-chain expert. With the aid of the new free-of-charge and freely accessible online tool, users can design their energy chain system using a smart phone, tablet or a desktop computer. Whether an unsupported, gliding or hanging application, the configurator determines the energy chain that is optimally suited. To do this, the user simply has to open the e-chain expert (www.igus.eu/e-chain-expert) select the unharnessed or harnessed cables, enter the application and environmental parameters, decide on the appropriate energy chain from a pre-selection and configure it. In the energy chain configurator, the user can choose from over 1,300 highly flexible chainflex cables tested by igus as well as over 4,200 harnessed readycable drive cables. These are tested and, like all igus cables, come with a 36-month guarantee. On the basis of the specified cables and the application data such as installation space, movement and environment of the energy chain, the customer can choose from a selection of 150,000 e-chain parts for the most cost-effective solution. All igus products are tested in our own 3,800 square metre laboratory. |