Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ? |
50 percent lighter: the world's first modular igus hybrid chain made of steel and plastic18.06.2019
Cherry pickers, construction machinery and lifting platforms have an identical challenge to face: a safe and compact vertical guidance of the cables and hoses. For such scenarios, users usually rely on tough and rigid steel chains. However, these are very heavy and difficult to install, and often need to be completely replaced when service or repair is called for. This means immense costs for machine operators and hiring companies due to equipment downtime. igus has now developed a hybrid energy chain especially for high unsupported travels. The supporting chain links of the new energy supply solution are made of steel and ensure high rigidity, whereas the pin/bore connection, the outer links and the crossbars are completely made of a tribologically optimised high-performance plastic. Thanks to the plastic - unlike a steel chain - the user saves 50 percent weight. Compared with a plastic energy chain, the new hybrid energy chain can implement 50 percent more unsupported length. |