La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.
Presse |
|
Avete qualche richiesta? Avete bisogno di materiale? Le informazioni aggiornate per la stampa e il materiale fotografico pronto da pubblicare sono disponibili per il download qui. Contattateci telefonicamente, via e-mail o fax! |
|
Contatto stampaVolete essere aggiunti alla nostra lista di distribuzione per i media? |
Wear-resistant sliding movement in an extremely small space with iglidur tribo-polymer coating from igus13.08.2019
More and more compact, lighter and smaller: this is not only the slogan of electronics manufacturers; in industry as well, the demand for space-saving machines is growing unceasingly. As a consequence, technical design engineers are creating small machines and equipment for use where installation space is at a premium. As regards components, more solutions are called for in the area of plain bearing technology as every single millimetre counts. In order to meet the new requirements in the area of mechanical engineering, igus has made use of its decades-long experience in the development of tribologically optimised plastics and has now developed three new maintenance-free and lubrication-free tribo-polymers as coating materials specially for very small installation spaces. As a result, not only the lubrication-free iglidur plain bearings but also the iglidur coating service for metal surfaces with the material iglidur IC-01 and the new IC-02, IC-03 and IC-06 materials are now available to the user.
|