Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
Lubrication-free adjustment: polymer rollers assist igus' hybrid linear system17.04.2020

Hybrid roller bearing with tribo-polymer sliders halves coefficient of friction in lateral position

In order to move doors, monitors or even panels, users rely on lateral installation of the linear systems. To enable the linear guides to absorb these lateral forces better, igus has now developed a new hybrid linear system. Two hybrid bearings provide low-friction adjustment with polymer rollers and tribo-polymer slide elements. Combined with an easily fit rail adapted to the new roller bearings, igus offers a cost-effective and visually appealing complete solution.


In the packaging industry, furniture technology or even in machine tools: drylin linear guides can be found wherever movement is required. On tribologically optimised liners, the linear carriages slide on the rail, ensuring precise and long-lasting adjustment. If a low driving force is required for manual adjustments, rollers are used in the bearing element. Especially for a lateral installation, the position of the rollers for the force absorption is crucial. As a solution for such applications, igus has now developed two new hybrid roller bearings, which offer smooth adjustment with low drive forces and maximum support at the same time. The WJRM-41-10 has two offset polymer rollers with optimised alignment for better force absorption and easier rolling. The hybrid roller bearing WJRM-31-10 with single roller is in turn the matching, supporting bearing on the opposite side. By using the two roller bearings, the user can minimise the coefficient of friction by half and increase the service life of the application. In both bearings, in addition to the rollers, there are sliding elements made of the low-friction tribo-polymer iglidur J. The lubrication-free and maintenance-free material is characterised primarily by its low coefficient of friction in dry operation. Both bearings can be positioned at the desired bearing clearance. These are very cost-effective if the bearings are produced in the zinc die-casting process.

Smooth adjustments with low-friction
Using a top plate, the two new roller bearings can be expanded to a linear carriage. To ensure that the bearings can also be used on the appropriate guide, igus has developed a low-profile hybrid roller rail. This has a special geometry optimised for the hybrid roller bearing. The rail has a simple design without visible holes and is able to attach from the back with sliding blocks. This makes the new rail in combination with the hybrid roller bearing ideal for lateral installation, for example in kitchen and furniture construction as well as in machine tools or in jig construction.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH