Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
Advancing research: igus is a new member of the Profibus Nutzerorganisation e.V.08.10.2020

Tested chainflex Profinet cables ensure reliable data transfer in moving applications

Profinet is the world's leading Ethernet-based communication solution for industrial automation. Because even large volumes of data can be transferred quickly and safely thanks to real-time communication. In order to advance the research of Profinet technology in moving applications, igus has now joined the Profibus Nutzerorganisation e.V. as a cable specialist.

According to the results of a study by IHS Markit, Profinet is the industrial Ethernet communication system. Based on the newly installed nodes, Profinet achieved a market share of almost 30 per cent in 2018. The technology was developed by the Profibus Nutzerorganisation e.V. (abbreviation PNO). "Due to the increasing importance of Profinet in moving applications in industry, we have now joined the Profibus Nutzerorganisation e.V. as a cable specialist. Here we want to further advance the development of the technology", says Andreas Muckes, Head of chainflex cables Product Management. "So the customer can be sure that our cable solutions always meet the current electrical requirements." Profinet offers clear advantages for industry: a large amount of data can be transferred at up to 100 Mbit/s based on the Ethernet protocol. However, this also means that machines and cables must move increasingly more dynamically in a compact installation space: a challenge for standard cables. Therefore, igus has been developing cables that are specifically suitable for use in energy chains and on robots for over 25 years. For Profinet alone, igus offers nine types of cable for different application scenarios.

Whether linear movement or torsion, the cable is guaranteed to last
The chainflex Profinet cables are available in four jacket materials, four bend radii and two torsion angles. The igus product range offers solutions for small installation spaces, maximum speeds and three-dimensional movements with up to ±360 degrees/m on the robot or in free movements. The cables have a number of approvals such as UL, NFPA, EAC and CTP and are available in desired lengths directly from stock. All cables also undergo an extensive series of tests in the company's own 3,800 square metre test laboratory. There, for example, the Profinet cable CFBUS.LB.060 completed over 65 million strokes with a bend radius of 63mm. Thanks to the numerous laboratory results, the chainflex cables have a 36-month functional guarantee, which is unique in the world. Upon request, they are also available fully harnessed as readycable, for example with an M12 round connector from Telegärtner.

More information on Profinet technology and chainflex Profinet cables is available at https://www.igus.in/info/unharnessed-cables-profinet


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH