Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Linear carriage-to-go: assemble and disassemble igus linear unit in just one step21.04.2022

The new drylin concept is very easy to handle and saves a lot of time

The motion plastics specialist igus demonstrates an exciting new approach for linear carriages. A clip mechanism enables easy installation and removal from the linear guide in a matter of seconds.


Whether building technology, mechanical engineering, industrial handling systems, measuring and testing technology or camera technology: linear systems are an integral part of everyday life. The principle is always the same: a component, such as a control panel, is installed on a carriage and moves over a linear profile with the aid of a guide system or a rolling guide. Previously, it has only been possible to remove the carriage with some effort. Often only using tools and usually only via the profile ends, provided the installation space permits it. A design limitation where tractor manufacturers wanted an alternative solution. For example, the demand is for a carriage enabling operators to keep their touch displays in the optimal view position. There is also a requirement for it to be removed easily and safely in one step after finishing work. They can be stored safely, protected from theft, moisture and cold. "Inspired by this need, we developed the linear “carriage-to-go” as part of a design study - a carriage that can be removed from the linear rail without tools and from any position in just one step," explains Michael Hornung, Product Manager drylin Linear and Drive Technology at igus. "In the field of linear technology, this idea is a novelty that saves time and opens up new areas of application."

Intuitive operability ensures fast installation and removal
The operation of the clip carriage is simple: the carriage moves on a double profile rail via four lubrication and maintenance-free high-performance plastic slide bearings. If the user pulls a lever on the underside of the carriage, two bearings open via a spring mechanism. The carriage can now be pivoted off the rail and removed. The installation is just as quick. The user places the carriage on the upper rail and clips it onto the lower rail. "Operation is so intuitive that installation is reliable and quick." says Hornung. The first pilot customers are enthusiastic about the new technology. Among these customers are users of camera systems and measuring and testing technology. You can install cameras and evaluation units on linear guides faster than ever. The design study is therefore becoming a product. The market launch is planned for spring 2022.

Clip carriage expands the drylin W product range
With the new clip carriage, igus is expanding the drylin W product range. There are currently more than 50 different versions of linear guide carriages, which, in combination with other design elements, allow an almost unlimited number of variants. The essential feature of all models is that they enable high accuracy and smooth operation due to the high-performance plastic used in the plain bearings and that they can be cleaned quickly and thoroughly due to the absence of lubricants.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH