Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
STS container cranes: fit for the future thanks to the new igus heavy-duty rol e-chain24.08.2022

P4HD.56.R: suitable for long travels, high speeds, heavy cable loads and Industry 4.0

Container cranes in ports around the world will be even more powerful and fail-safe in the future. This is due to the fact that igus is launching P4HD.56.R - a new heavy-duty energy chain prepared for long travels, high speeds, heavy cable loads and Industry 4.0.


If your waistline expands, you need a new pair of trousers. Something similar is happening in ports around the world. Modern container ships are huge - take the Ever Ace, which is 400m long, 62m wide and loads almost 24,000 containers. The new trousers in our comparison are a larger ship-to-shore (STS) crane that loads and unloads the containers. This enlargement also affects the energy chains that guide the energy and data cables for the crane trolley on the crane bridge. They have to withstand unprecedented loads: travels of over 130m, cable weights of up to 10kg/m (over 20kg/m for motor-driven trolleys) and accelerations of more than 1m/sec2 are standard for Triple E-class STS cranes. In other applications, travel distances of several hundred meters, cable loads of up to 50kg/m and accelerations of 8m/sec2 and more can be achieved. "We have developed the new P4HD.56.R heavy-duty energy chain for these extreme requirements," says Theo Diehl, Industry Manager for Cranes at igus. "The energy chain is particularly robust and, thanks to its sensor technology, prepared for Industry 4.0 trends, such as predictive maintenance. This combination significantly increases STS crane reliability."

The heavy-duty energy chain is to run trouble-free for up to 15 years
The engineers have come up with special design features to achieve a long service life in STS cranes under high loads. "A special fork-tab principle ensures even greater stability at higher additional loads, while a pin/bore connection made of tribologically optimised plastic minimises wear," says Diehl. Furthermore, rollers are mounted in the inner radius of the chain links. If the e-chain folds, the upper run rolls on the lower run instead of sliding. Thanks to the low coefficient of friction, payload and acceleration can be increased without changing the push/pull force. Long-term tests in igus's in-house laboratory prove that P4HD.56.R, the heavy-duty design, achieves a 50% longer service life than the normal P41.56R variant. "Our goal is for the e-chain systems to run on any STS crane for up to 15 years - trouble-free and with minimal maintenance," says Diehl. A nice side effect: the rolling movement reduces the required drive energy by 57%. This is another advantage in times of rising energy prices. Since crane systems also require robust cables that can be used to realise long travels with high dynamics, igus also offers CFCRANE, a chainflex cable range that has been specifically developed for crane applications.

Fit for Industry 4.0
But the new P4HD.56.R is not only robust, durable and energy-saving. The heavy-duty energy chain is also suitable for Industry 4.0. For example, it allows predictive maintenance. With the help of i.Sense monitoring sensors, the chain link status can be continuously transmitted to the i.Cee:plus communication module. i.Cee allows usage-based and condition-based maintenance, extending inspection intervals. Maintenance is necessary only when the system sends a signal to that effect. Operators of STS cranes can use the i.Cee system to greatly increase system availability and extend energy chain service life. Holiday shut-downs and other planned downtimes are automatically taken into account in the i.Cee service life calculation, and the forecast is constantly checked with sensors. All these advantages do not limit usable inner width because the condition sensors and their electronics are integrated into the rol e-chain links to save space. No additional cables are necessary because data is transmitted via radio. "The new P4HD.56.R-series e-chains thus meet all the requirements that apply to STS cranes of the next generation and the generation after that," says Theo Diehl.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH