Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Fast set-up of motor control systems from igus: no lengthy programming27.01.2023

igus accelerates the commissioning of drylin E motor control systems with free motion sample programmes

The programming of motor control systems and the integration into machine environments often takes several days, amounting to costs of several thousand euros. A barrier that the Cologne-based company igus is now removing. With the free motion sample programmes, it is possible to commission the dryve series motor control systems in just a few minutes, and connect them to higher-level programmable logic controllers (PLC). This benefits automation newcomers and professionals alike.


The level of automation is rising rapidly in many companies. The workload for technicians and engineers responsible for programming and synchronising automation movements is increasing accordingly. "To ease the burden, you can download sample programmes for our dryve motor control systems for free," says René Erdmann, Head of Business Unit drylin E Drive Technology at igus. Customers worldwide mostly use the cost-effective control systems for comparatively simple automation tasks - such as for controlling DC, EC and stepper motors in single axes, line robots, flat linear robots, room linear robots and delta robots. "Thanks to the ready-made sample codes, users can now integrate our motor control systems into higher-level PLCs and machine environments in a flash, and define motion sequences in a time- and cost-saving manner." The sample programmes are compatible with PLC manufacturer Siemens, but also with industrial PCs, microcontrollers, such as Arduino, and single-board computers, e.g. Raspberry Pi. Further sample programmes for Beckhoff, Wago and Eaton are already being planned.

User saves several days of programming work
Access to the sample programmes is barrier-free: users can find videos on the igus website that show the most common automation movements - such as a trolley moving to different target positions on a linear axis. If the motion programme seems suitable, the user can download the software code and load it into the master control system. The motor's actions can then be parametrised and adapted to individual requirements via an intuitively understandable graphic interface. No programming knowledge is required to set travels, target positions and accelerations. The advantage is obvious. "Initial customer feedback confirms this: with some sample programmes that map more complex motion sequences, users save several days of programming work," says Erdmann. So far, the range includes 19 sample programmes that are suitable for positioning tasks, testing and experimenting devices, pick-and-place handling, automatic assembly machines and feeding systems. "In future, we will continuously add motion programmes to the range that customers need most frequently. If users can't find a sample programme, e.g. for a special application or for a different master control system, they can request it at the igus website."

Instructional videos accelerate commissioning of the motor control systems
In order to further accelerate the commissioning of the motor control system, igus has also implemented the so-called dryve experience in addition to the sample programmes - an online world as a supplement to classic analogue media. Instead of reading printed operating instructions, customers can learn how to use the motor control systems with videos. Erdmann: "The short films deal with topics that customers most often ask our telephone hotline about, such as connecting brakes to the motor control system. With the videos, they now have new, easy-to-understand 24/7 support." All relevant digital documents for a smooth commissioning of the motor control systems - including firmware, EPLAN macros and 3D drawings - are also available online.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH