Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
igus energy supply, the only one of its kind in the world, makes jib cranes safer11.05.2023

Space-saving, durable and cost-effective: guidelok swing is to establish itself as an alternative to classic festoons

Energy and data cables hanging from jib cranes often pose a great risk. Careless movement of loads, forklifts or other slewing crane systems in the immediate vicinity can cause them to become entangled and torn off. igus has therefore developed the guidelok swing, the only energy supply system of its kind in the world. It can be installed directly in the T-beam contour, and a special rocker system allows it to be used for long beam lengths cost-effectively with little wear. This significantly increases operational safety.


Jib cranes are an indispensable part of industry. They transport workpieces of all kinds - to loading ramps, processing machines and assembly stations. However, failures can always occur - for example, when hanging cable loops are damaged by a forklift during workpiece unloading. The result is downtime, unplanned repair costs and even production delays. "To increase system safety and productivity, we have developed a new energy supply system called the guidelok swing," says Theo Diehl, Head of Industry Management Cranes at igus. "Energy and data cables no longer hang in the air, but move directly in the jib crane's girder contour thanks to the energy supply system's particularly slim, space-saving design. They stay out of the reach of lifted loads, industrial vehicles or other jib cranes."

A technical design trick ensures fail-safe operation
And this is how the system works: the energy and data cables are fitted in an energy chain made of high-performance plastic. The lower run rests on the T-beam flange and is connected to the trolley. Unlike traditional chain applications, the guidelok swing moves the lower run. The upper run is held above the trolley by the guidelok swing's rocker elements. A classic energy chain movement would normally involve the upper run gliding on the lower run. igus, however, has introduced a design trick: every 800 millimetres, rockers are screwed to the T-beam crossbar. When the upper run passes, the chain radius pushes the rocker flaps up and engages. In the opposite movement, the flaps open like a trapdoor and release the upper run again. The advantage is that the upper and lower runs never touch. Wear is therefore low, extending the energy supply system's service life. "Another advantage is that the guidelok swing eliminates the need for a guide trough, since the e-chain is held in position by the rockers and cannot break out sideways," says Diehl. "The energy supply system is therefore also cost-effective, since it costs about as much as classic festoons." Existing systems can also be converted more quickly because there is no guide trough.

The world's first users have been won over
SEW-Eurodrive is the first to use the new guide system. The German drive technology manufacturer has equipped an indoor crane with the guidelok swing at its plant in Gauteng, South Africa. The crane moves components for chemical cleaning with a high-pressure cleaner. "Initially, the engineers considered working with classic festoon systems," Diehl recalls. "But Sales Manager Marius Ferreira from our partner Stahl Cranes and Hoists quickly convinced them that the new guidelok swing guide system reduced the risk of accidents and increased crane reliability." The energy supply system not only prevents collisions with forklifts, but is also chemical-resistant and corrosion-free and requires no maintenance or external lubricants. SEW-Eurodrive is enthusiastic about the solution, as is an industrial company in South Africa, Barloworld, which has announced that it will work with Stahl Cranes and Hoists to gradually convert more jib cranes in its workshops.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH