Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Mon interlocuteur
Sélectionner un département

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

CH(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

e-skin flat ESD: for the highest level of safety and cleanliness in cleanrooms08.11.2023

igus is adding an electrostatically dissipative variant to its almost particle-free e-skin flat energy chain series

igus has added an ESD variant specifically for highly sensitive cleanrooms to its e-skin flat series. The modular ribbon cable's new material prevents the chain from becoming electrostatically charged while ensuring that it generates no particles, even during very fast movements. The modular design with individual pods also allows quick energy supply system filling.


In addition to particle-free cleanrooms, electronics and semiconductor industry production also requires machine components that are electrostatically dissipative. Even the smallest current surge from electrostatic charge can easily destroy the product. So, igus has added an ESD variant to its e-skin flat series. The new black e-skin flat is made of an electrostatically dissipative material. "The new material combines ESD approval, which is frequently required, with the proven e-skin flat's low particle emissions. The chain produces almost no particles and dissipates electronic charges directly," says Kira Weller, e-chain Product Manager at igus. "The new e-skin flat ESD gives us just the product our customers need to produce sensitive electronic components." The new cable is used by such companies as Weiss, an automation specialist, in its high-speed HP70 pick & place unit, which comes into play in such applications as material handling in the medical and pharmaceutical industries. Weiss is enthusiastic about the advantages of the e-skin flat ESD. The igus ribbon cable is much stronger and quieter and less susceptible to wear in quick movement than are classic corrugated hoses. The e-skin flat also features a modular design, unlike laminated ribbon cables made of polytetrafluoroethylene (PTFE). In the igus in-house cleanroom laboratory, which was developed with the Fraunhofer Institute, the new e-skin flat has already proven itself in the highest cleanroom class.

Easy cable replacement
"Single pod" profiles ensure quick, easy e-skin flat installation, so the energy supply system can be easily expanded. A zip-lock system allows easy cable replacement. "This is a big advantage over the widely-used PTFE ribbon cables, in which the stranded cores are welded in a continuous ribbon and cannot be separated. If a single wire breaks, users have to replace the entire system. That takes time and money," says Weller. "For our e-skin flat, we offer the CFCLEAN cable cores for transmitting energy, motor control, bus and Ethernet signals. This way, the user gets a ready-to-connect energy supply system directly from a single source." If longer travel distances (up to five metres) are needed, a support chain can be simply integrated into the pods. Spacers, connection elements from the e-skin flat series and the smart i.Cee EC.S ultrasonic condition monitoring sensor are also compatible with the new ESD chain.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH