Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Small & Light – The readychain rack light fits into even the smallest corner if the machine …26.08.2013

The igus assembly transport racks readychain rack and readychain rack light reduce process costs by up to 80 percent.

The light and slim assembly transport rack readychain rack light from igus now allows a perfect-fit, "plug and play" pre-assembled energy chain system to be used even for small applications. When combined with the already popular large readychain rack, the igus energy chain system readychain is finely tuned to customer requirements. Machine and plant engineers can reduce their process costs by up to 80 percent with the help of the readychain racks.

Modules are being used more and more often in mechanical engineering since their fixed prices allow manufacturers to plan more reliably. In addition, process costs are reduced through significantly shorter assembly times. This also applies to pre-assembled, tailor-made energy chain systems: The faster the energy supply arrives at the machine, the faster the mechanical engineer can do his job. For this purpose, igus has developed the variable assembly transport rack readychain rack. It delivers the plug-and-play energy chain system readychain quickly and safely to the machine. On site, telescopic supports are used to assembly it gradually and precisely to the machine interface within a single day. This helps to reduce process costs: Up to 80 percent in the prototype phase and up to 50 percent over the complete assembly process. It's no surprise that the assembly transport rack readychain is already being used in numerous mechanical and plant construction applications.

Small and finely made – the new readychain rack light
To make assembly even more efficient, the igus design engineers have made ongoing developments to the rack: With an edge length of only 40 millimetres, the new readychain rack light is only half the size of the original igus assembly rack which is too big for fine applications. The components of the new readychain rack light, such as the, crosses, T-pieces and telescopes are slim, so that the energy chain can be precisely fitted and used even for small applications in the last corner of the machine. If the large readychain rack is combined with the light version by means of adapters, adaptation of the readychain module to the individual customer application can be refined, making its use even more versatile and efficient.

Whether large or small, long or short – flexibility is the name of the game
igus is now in a position to use the readychain rack both for large and small applications. Regardless of their size, both racks are constructed in millimetre precision even at the prototype phase, yet they can still be modified later for series production. It used to be weeks or even months before products were ready for series production. La Adaptation at a later stage was impossible due to the welded parts. However now, in contrast, the length of the modular supports and braces of the readychain rack, which fit together perfectly and are telescopic, can be adapted at any time. If modifications to the machine make the addition of components necessary at a later date, the changes can be carried out at any time thanks to the latching mechanisms – without any welding or painting work being required. Another argument in favour of the use of readychain racks is their reusability. Every readychain rack can be dismantled into its individual parts which can then be put together again for another project.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH