Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
Equip for the future today with RoHS-compliant iglidur plain bearings14.07.2014

High performance plastics from igus meet EU directive and provide planning reliability

The extended EU Directive 2011/65/EC (RoHS II) became valid at the beginning of the year, therefore tightened the permissible limits for hazardous substances in more and more areas. From the 22nd July, products with unacceptably high concentrations, such as lead-containing plain bearings face extinction in the Medical Technology industry. igus offers iglidur polymer bearings as a RoHs-compliant alternative that promises legal and functional reliability to the manufacturer, and safe use and disposal to the user.

Since the mid-1990s, limitations on the use of environmentally hazardous substances were enforced for electrical and electronic devices and their components all over Europe. Steadily tightened guidelines under the abbreviation "RoHS", (Restriction of [the use of certain] Hazardous Substances) set limit values for the use of industrially-necessary but potentially harmful substances such as, chromium, lead, mercury or bromine. With the new RoHS II standard, a maximum value of 0.1% of the total weight is determined for most. Many manufacturers changed their production accordingly in the past, and others must now respond because exemptions, such as for the medical and control technology, will expire this month. Since similar regulations are also put in place in countries such as the USA, Japan or China, these standards must be met increasingly with a global perspective. However, metallic composite bearings often have alloys that are not compliant with RoHS.

Reliable planning and amendments with iglidur plain bearings
Customers, who consider the RoHS compliance, have an immediate alternative with iglidur bearings. This is because the substances covered by the Directive basically have no role to play in this material made of thermoplastic plastic compounds. Based on the principle of dry lubrication, the iglidur bearing technology uses tribologically optimised base polymers, solid lubricants and fillers of exclusively non-metallic and RoHS-safe ingredients. The provisions of the RoHS Directive are also subject to permanent review and thus there is the possibility of future revisions of the legal requirements. Manufacturers, whose equipment and components today fulfil the admissible limits, or are even excluded from the standards today, must expect a further tightening. iglidur polymer bearings provide planning reliability today. In addition to their “traditional” advantages of freedom from maintenance and lubrication, all igus products are without hazardous substances. RoHS compliance is therefore one of the natural features of iglidur plain bearings. The igus plain bearings are safe not only in terms of laws and regulations. By the option of life prediction and configuration using online tools, RoHS-compliant metal bearings can be replaced quickly and easily by iglidur plain bearings.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH