Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
Sliding and rolling: igus hybrid linear bearings in new sizes02.02.2015

drylin double roller hybrid bearings now available for rail diameters of 10 and 16 millimetres

Cologne, 2 February, 2015 – igus, The Cologne-based specialist for lubricant-free bearing technology; has expanded its range of double roller hybrid bearings with two new sizes. The range of hybrid bearings will now be completed with sizes of 10 and 16 millimetres. Lighter and quieter linear running on two rollers -- also for applications with reduced installation space.


The quiet and smooth-running hybrid linear bearings from igus are used not only in camera technology, sliding doors or machine tool doors, but increasingly in cabins for construction machinery, or even for the individual hobbyist's needs. To facilitate the design engineer in their selection, there is the option of two additional sizes of hybrid carriage. Behind the innovative concept of this bearing from igus is the combined advantages of plain and roller bearings. For extremely smooth and almost silent operation, the concept provides two angularly opposed rollers made of maintenance-free high performance plastics. The rollers take the weight in the main load and ensure low driving forces for manual operation. When misuse or moment forces occur, they will be absorbed smoothly over the sliding element,. thus eliminating the risk of the carriage leaving the rail at the same time the movement of heavy loads becomes possible with minimal effort - all absolutely free of lubricant.

Suitability for the design of smaller installation sizes
"The hybrid bearings available with 20 mm diameter have already proven themselves in practice," says Stefan Niermann, head of the drylin linear and drive technology division at igus. "If only one guide rail is necessary, the user saves considerable space. In this aspect we have now gone one step ahead and offered the double roller hybrid bearings in new, smaller installation sizes of 10 and 16 millimetres.” These allow the design engineer now an even more flexible installation of the bearings, such as for control panels or stage setting installations on double rails and in combination with a complete carriage. Since the hybrid bearings encompass more than 180 degrees, they can also be used on simple shafts.

Ideally suited for manual operation.
Due to the low friction of the hybrid bearing, the required displacement force could be reduced by factor 5. They are therefore ideally suited for manual operation. Since loads up to 100 kg can be easily moved manually, they are ideal for applications in the furniture and office equipment industry (for example, sliding doors) as well as camera and monitor installations. The double roller bearings, which are priced lower than the common rolling solutions in the market, offer an efficient solution and can be ordered as a separate bearing carriage, or as a completely pre-assembled hybrid carriage.

A video of the operation of the double roller hybrid bearing from igus can be viewed at http://www.igus.eu/doublerollerhybridbearing


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH