Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
igus presents a new energy supply system10.02.2015

guidelok slimline P for less weight and more dynamics saves up to 80 percent of the cost

To be able to always achieve faster accelerations and speeds in aisle travels, igus has developed an energy chain supply system completely made of plastic. This is characterised by low weight and moreover, easy installation. Visitors to the igus stand at the Hanover Fair in Hall 17 can experience this innovation and more "motion plastics".


igus has advanced its guidelok slimline system once again and now presents the new GLSL-P, which is entirely made of plastic. The guide system for hanging energy chain applications does not require an enclosed channel trough or other elaborate, expensive enclosures and holds the energy chain system as in aisle travels on the railway. Instead, lightweight plastic segments are mounted only every two metres, which saves up to 80 percent trough costs and also weight compared to the previous metal option. Therefore, even faster speeds and accelerations can be achieved. Another advantage of the plastic novelty is that vibrations are absorbed better. "The lightweight guide rails made of fibreglass can easily be plugged into the plastic segments of GLSP-P, hence, implementing the installation completely without tools, leading to a reduction in costs yet again," explains Christian Strauch, industry manager for materials handling at igus.

Secure hold for energy chain system
Two automatically actuated compensators in the segments of the guidelok slimline P fix the e-chain and ensure a quiet, smooth run. If the chain moves in the radius through the segment, the compensator is activated and fixes the energy chain. The innovative locking levers are complemented by open guide rails made of reinforced plastic between the segments, which allows for more dynamics.


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH