Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
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
Hannover Messe: on route to a 1,000 euro robot with igus19.03.2015

The next generation of the modular joint robotic systems offers flexibility and reduces costs

Reduce costs and improve technology: this is the promise of plastic specialists, igus, and it has now taken a further step in this direction in the field of robotics. At Hannover Messe, the Cologne-based company will exhibit the next generation of robolink D, a direct driven articulated arm made from plastic and aluminium that can be used to build a 4-axis robot from 1,500 euros.


Last year, igus presented its new robolink D product range. In this system, a robolink articulated arm is driven directly by a motor that is attached to the axis. During this process, robolink D uses a lubrication-free igus PRT polymer slewing ring bearing, which is installed in plastic housing. This bearing is now also available as a full polymer version. The bearing is driven by a worm gear drive with the option to add an igus stepper motor Nema 17 or 23. The robolink D joints are available in three sizes and can be combined with components made from plastic or aluminium to form articulated arms with one to four axes. “The modular combination of the robolink articulated arm, the motor and the drive creates a customised and configurable robotic system”, explains Martin Raak, robolink Product Manager. “The construction kit is light and highly flexible. This makes it interesting for not only robot manufacturers and machine and equipment builders but also system integrators and automation specialists from all sectors, from automotive production to medical technology. This particularly applies when dealing with humans-machine interaction.”

Robots from 1,500 euros

Thanks to advances in development and production, it is now possible, depending on the batch size, equipment and load capacity, to use robolink D to develop a 4-axis robot for between 1,500 and 2,500 euros. This includes the motors and the appropriate cables. Both the individual components and the pre-assembled system with construction diagrams can be ordered. The load capacity is up to 4 kg – with a system weight of just 5 to 8 kg. The motors can be controlled using conventional control modules. “In the future, it should also be possible to use a lower cost and simpler motor control involving a web browser, as igus is currently exhibiting at Hannover Messe for the first time for all drylin E linear axes”, comments Raak, offering an insight into how the system is set to develop. This new solution is compatible with many different industrial control systems thanks to CANopen and digital inputs and outputs. “Our aim is to continually develop the robolink D system and thus reduce costs even further so that it becomes possible to construct a 4-axis robot from 1,000 euros in the near future.”


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH