Selezionare la località di consegna

La scelta della pagina del paese/regione può influire su diversi parametri, come prezzo, opzioni di spedizione e disponibilità del prodotto.
Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale, vi assegneremo immediatamente il personale di riferimento per l'assistenza.

CH(IT)

Compact cable guidance in innovative impregnation system for electric motors

Rotating energy supply and chainflex cables for impregnation processes in the automotive industry

To enable high-quality impregnation in the production of electric motors in the automotive industry, VAF GmbH has designed an innovative new system. Today, it enables higher unit output and reduced air and energy consumption with a smaller space requirement. A plastic energy supply system was also able to contribute to the ambitious concept, ensuring reliable guidance of the internal chainflex cables in continuous operation in a confined installation space.

Profile

Multifunctional hall This line for impregnating electric motors achieves a 25% higher number of production pieces with a 45% more compact design.

Problem

This innovative and newly patented system for impregnation from VAF GmbH is intended to set new standards. It is used in the automotive industry in the mass production of electric motors and is used to insulate electric motors to increase their durability and performance. It has been designed for the application of high-quality insulation especially in the field of high-voltage drives. The stators of the electric motors are treated in the machine based on the hot dip impregnation process. In this process, the stator windings are heated via current heat, which requires up to 1,000 amperes per phase. The energy supply for supplying the current heat should allow a pivoting movement of 180°. Since the machine is to take up as little space as possible in the customer's production halls, the energy supply also had to meet particularly tight space requirements. And both the cables and the cable guidance had to be for reliable continuous operation and guarantee a high degree of planning security. Since OEMs process quantities of around 1,000 to 2,000 electric motors per day and per product, a breakdown would be very costly.

Solution

The innovative concept was implemented using an E4.1 energy chain (E4.80 series) and chainflex motor cables running in it. The plastic energy chain is highly rigid and resilient, allowing it to perform reliably over the long term even in hot environments, high aerosol content in the air and continuous operation. Equally important was the small space requirement. Therefore the cable guidance was designed as RBR chain, that is an energy chain with reverse bend radius. It rotates in a compact rotary module and allows the required rotation of 180°. All cables, including the energy chain, were supplied as a pre-assembled complete system - a so-called readychain energy supply - ready for installation. This saves installation time and costs. The energy supply system has thus become an important part of the plant's new concept, which envisages a particularly efficient system with higher output from a smaller space requirement, lower energy requirements and reduced air consumption. And this has also been achieved: the number of production pieces could be increased by up to 25% compared to comparable machines, with a 45% more compact design and 80% less air consumption.

Energy chains
Energy chains

motion - magazine for energy chain systems®

Tech up ... Cost down

This awards booklet contains real life examples of how customers have improved technology and saved money using energy chain systems for cable management.
Order your personal copy here


I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® GmbH legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® GmbH o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® GmbH dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® GmbH