Irrigation system: long travels

Roller energy chain enables the precise and long-lasting operation of this irrigation system

A precise watering trolley significantly reduces the use of irrigation water and fertiliser in potted plant cultivation in the field. The corrosion-resistant guidelite trough system together with the E2/000 series ensures an economical water supply over a travel distance of ten to 200 metres.

Profile

  • What was needed: E2/000 energy chain of the 3500 type as roller energy chain, guidelite guide trough
  • Requirements: precise movement, use in wind and weather, long travel of 200m
  • Industry: agriculture
  • Success for the customer: the roller energy chain ensures precise and safe travel over the long travel distance whilst reducing the drive power required to move the chain to less than 25%.

Problem

This exact casting trolley is used outdoors for pot plant cultivation. It was developed by Rathmakers Gartenbautechnik GmbH in co-operation with the NRW Chamber of Agriculture. Its advantage: the system waters - as the name suggests - very precisely only the pots and does not waste water on the areas between the plants. This means that water is only used where it is needed in cultivation, and the savings potential is usually over 50%. The heart of the exact casting trolley is a long rail that runs lengthwise exactly between two fields. It is on this rail that the exact casting trolley is installed on a carriage. An elongated structure extends from this trolley on both sides, overhanging the fields. When the trolley travels on the rail, the frames also travel over the fields and can water the pot plants via inner-lying cables. A windproof, weatherproof and precise solution was sought for the cable guidance.

Solution

The cable guidance of the various cables required for the exact casting trolley is today ensured via two essential components. On the one hand, a corrosion-free guidelite trough system is used. These guide troughs are usually used on particularly long travels as well as in rather slow applications with low cycle numbers. An E2/000 energy chain of the 3500 type travels in it. It is suitable for the medium load range and safely carries the various cables over a travel of ten to 200 metres. Other special features of the quietly operating energy chain are its high stability and long service life. Despite the slow travel speed, it ensures a particularly precise carrying of the cables. This is also ensured by the rollers on which the chain travels. The roller energy chain has the advantage that it reduces the drive power required on the long travel to less than 25% to move the chain.

Irrigation system
Irrigation system

Here, you can find further interesting applications from very different areas of use

To the vector award



I termini "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "energy chain", "energy chain systems", "e-loop", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" e "yes" sono marchi registrati di igus® SE & Co. KG legalmente protetti nella Repubblica Federale Tedesca e, ove applicabile, in alcuni paesi esteri. Si tratta di un elenco non esaustivo di marchi (ad es. in corso di registrazione o marchi registrati) di igus® SE & Co. KG o di società affiliate a igus® in Germania, nell´Unione Europea, negli Stati Uniti e/o in altri paesi o giurisdizioni.

igus® SE & Co. KG dichiara di non vendere prodotti delle aziende Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber e tutti gli altri produttori di sistemi di azionamento menzionati in questo sito web. I prodotti proposti da igus® sono quelli di igus® SE & Co. KG